Hello,
should the pins of an unused driver stage be unconnected/open?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
should the pins of an unused driver stage be unconnected/open?
Regards, Holger
Anuj,
ok. In the User's Guide on page 33 it says unconnected:
If the half-bridge is used to implement only a high-side or low-side driver, using the VDS overcurrent monitors is
still possible. Connect the SHx pin as shown in Figure 21 or Figure 22. The unused gate driver and the
corresponding input can stay disconnected.
Is both ok?
Regards, Holger