Hi at all
For a project where precision and speed are needed, I designed hardware with DRV8711 and MOSFETs equal to those of the EVM-DRV8711 demo board.
With our MCU ATSAM3X8E I set the calculated parameters with your formulas and sent them via SPI to the driver.
I did several tests but the noise of the engine is a bit high. And I also burned 2 stepper motors for overheating.
I want to avoid it happening again and so I ask you for help from the Forum and technical support.
the stepper motor is Sanyo Denky brand
store2.lipsiasoft.com/.../706172_103-H7823-1740.pdf
bypolar motor, 1.8 ° per step, 4A, Resistance 0.65 ohm, inductance 2.4mH
the power supply is brand Mean Well mod. HRP-600-24
600Watt 24 Vdc
We have to have the highest possible torque at 128 uStep with low noise and temperature ...
I hope in your help
Thank you