Hi,
I choose DRV10970 driver for Faulhaber motor EN-1226 (9W).
And I have a problem with current signal form, it's not looks like in you datasheet (see photo).
Can you confirm that I use right driver or I have to be changed it.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I choose DRV10970 driver for Faulhaber motor EN-1226 (9W).
And I have a problem with current signal form, it's not looks like in you datasheet (see photo).
Can you confirm that I use right driver or I have to be changed it.
Thanks.
Dima,
Yes higher frequency should help. Unfortunately the DRV10970 cannot run at higher frequency, but we do have a recommendation for you.
We would recommend trying the DRV8323RS which can run at higher frequency, there is an EVM available here: http://www.ti.com/tool/boostxl-drv8323rs
The "R" version has an integrated buck regulator which will generate your 5V or 3.3V board rail from the VIN of around 15V as shown in your scope images.
This device has three current shunt amplifiers which can be used to read the current through each motor phase if desired, the DRV8320RS does not have these if they are not needed.
The "S" version is SPI controlled while there is also an "H" version which is hardware controlled if desired.
Please let us know if this recommendation suits you.
Regards,
-Adam