What is the TESTED minimum and maxium rpm that I can expect to achieve with the 8308 EVM and the included BLDC motor? What frame is the motor?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the TESTED minimum and maxium rpm that I can expect to achieve with the 8308 EVM and the included BLDC motor? What frame is the motor?
Thanks
Adam,
Prior to my message to you I had already read the EVM doc, no specs for the motor are listed concerning the RPM or the model number. But with your response I looked in the doc again, two more times. I do not see any specs on the motor listed, just that its a Telco Motion motor, but they manufacture many. And if I had a motor I would have looked and not bothered posting a message here.
Anyway it would seem to me that the design of EVM would determine the lowest and highest possible RPM for the motor, I don't care about the RPM limit of the INCLUDED motor, the document states the EVM can be used with other motors. So again, please I would like to know the design limits of the EVM's RPM. This is going to determine whether or not I am going to purchase the EVM. This is something that I would expect the engineer of the EVM would know.
TIA
TI has this listed as THINKS RESOLVED, but my questions are not Resolved. The available EVM doc does not list any motor specs. And since I requested the motor frame size it could be assumed that I did NOT have a motor,
Otherwise I would have measured it and also known the RPM parameters of the EVM, and not posted here. I thought my questions were not too complicated to answer fully instead of being redirected to nowhere. If someone could help me with my presale questions it would be greatly appreciated.
Thank you.