Other Parts Discussed in Thread: DRV10983, DRV10975
Hello,I found DRV10987 can drive 3phase brushless motor at a constant speed with easy way such as PWM,I2C and Analog input.
1. Could you tell me whether the maximum rotation speed is difference according to the control way or not?
2.when I choose the I2C for speed control,I need to set the register of motorspeed1:0x11 and motorspeed2:0x12 .
and We can set 0x00~0xFF in the registers.
if both motorspeed1 and motorspeed2 are 0xFF,motorspeed is calculated as below:
65536/10=6553.6Hz →6553.6Hz*60sec=393216rpm
I think it is not possible to drive the motor at 393216rpm because of hardware limitations.
Could you tell me what is the maximum rotation speed with I2C control ?
3.when I choose the PWM for speed control,I need to set the maximum speed with the register of SpeedCtrl1:0x00 and SpeedCtrl:0x01.
and We can set 0x00~0x1FF in the registers. What is the unit of the number?
Could you tell me how can I calculate the motor rotation speed?