We're seeing in some circuits with the DRV8303 that even that the EN_GATE is LOW the current consumption of the DRV8303 is higher than the value indicated by the datasheet.
We're unable to measure directly on each pin of the DRV8303, but we calculated the sum of current consumption on pins PVDD, SH_A, SH_B and SH_C pins. We're observing 2 patterns, in some DRV8303 we're obtaining a current around 4mA, in fact we observe that the total impedance is around 3kOhm. In other cases we are observing current consumption up to 12mA corresponding to an impedance of 570 ohm
Since there's no mention on the impedance of SH_A, SH_B and SH_C on the datasheet, could you give us an estimated impedance or current consumption on those pins where the EN_GATE is LOW?