This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: LAunch pad with DRV8301

Part Number: DRV8301
Other Parts Discussed in Thread: TMS320F28069, , CONTROLSUITE, LAUNCHXL-F28069M

Dear Sir,

I am currently working on  Close loop control of Switched reluctance motor.  I have purchased TMS320F28069  launch pad and DRV 8301 Booster -Xl evaluation board which sits on the launch pad.

I am not able to rotate the motor as there is no outputs from the Motor drive ic where as input is getting the pwm what i have programmed in the launch pad. I feel some initialisation problem during the startup.

Exactly what all to be done when we position the piggy board on top of launch pad.

Can you give the checklist of how the program is to be written with respect to drv8301?

And also Is that SCI interface of drv 8301 is a mandatory to be connected with micromcontroller.

pl send any sample codeor supporting software to quikly view the results

Thanking you in anticipation

Warm Regards,

S.M.Sundari

  • You may download the controlSUITE as the following link,

    https://www.ti.com/tool/controlsuite

    You can find an example project about the F28069 launchPad in the below folder.

    C:\ti\controlSUITE\development_kits\LAUNCHXL-F28069M

    And you can find an example project about how to use F28069 + DRV8301 to drive a 3-phase PSMS, you may just need to change some device configuration for F28069 launchPad since the example is based on F28069 controlCard.

    C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\PM_Sensorless