Hi team,
Could you please tell me why there 're some components which are not assembled on the EVM ? Such as C25 /C26 .
And What does these components do?
Regards,
Jhon Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please tell me why there 're some components which are not assembled on the EVM ? Such as C25 /C26 .
And What does these components do?
Regards,
Jhon Chen
Hi Jhon,
The DRV8432 is designed for motor control and other applications. The EVM arrives configured for motor applications.
C25/C26 and other capacitors can be populated to configure the EVM for applications like a TEC or LED lighting driver.
Please refer to Figures 15 and 16 in the DRV8432 datasheet for motor connections and Figures 17 and 18 for TEC and LED lighting connections.
Hi Rick,
Could you please explain more specifically about the function of C25 or C26?
Thank you very much!
Regards,
Jhon CHEN
Hi Jhon,
The capacitors are used to create a DC voltage. This would be similar to a switching regulator where one output creates a voltage and the other is set to 0V.