Other Parts Discussed in Thread: DRV8873
I'm looking into using this chip for several different applications on the same board with a 24V supply, so would use multiple modes. Is there additional info on exactly what each PWM input does in each mode?
One mode (mode 2) is the parallel H-bridges for a high-current TEC (~3.8A steady state), where only PWM_A and PWM-B inputs are used. In this case, what do the outputs do in the 4 possible input states? Most motor controller datasheets have a table for this.
I'm also driving 3 TECs cold-only (around 2.6A steady-state), so I'll just drive them from an H-bridge(s) to ground. I'm trying to drive two of them per DRV8412. Is it possible to combine two H-bridges in parallel (with the load to ground), then tie the other two in parallel for a different TEC? It's not clear to me what the differences between DRV8412 modes 0, 1, and 2. Mode 1 is out because I'd like current-limiting. How do the PWM inputs operate in modes 0 and 2? I'm looking for the same motor controller input/output table.
The DRV8873 is much better documented, but can't handle much current before the die overheats (according to the datasheet thermal calculations of Power(Rds-on) + Power (switching) at 80kHz). I wanted to use one of these to drive two of my cold-only TECs (independent mode), but the chip would be very near its max die temperature according to the power calculations.
Thanks for any help on this.
- SteveP