This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DRV8837: Sinusoidal output current?

Intellectual 1565 points

Replies: 3

Views: 116

Part Number: DRV8837

Is it possible to achieve a sinusoidal o/p current from the DRV8837 by modulating the PWM drive?  Or would another device be more suitable (5V Vcc, 1.8A pk)?

Regards

Jim

  • Hi Jim,

    Yes, it possible. But the DRV8837 may not be the best device depending on the application.

    Can you provide more details on your application?

    What load are you driving?
    What is your desired PWM frequency?
    What features of the DRV8837 are desired?
    Any other information?

    Best Regards,
    Rick Duncan
    Motor Applications Team

  • In reply to Rick Duncan:

    Hi Rick

    See below:

    What load are you driving? DC Motor

    What peak current do you require? 1.2 A peak, 0.9A RMS

    What is your desired PWM frequency? 1kHz

    What features of the DRV8837 are desired? Sleep Mode

    Any other information? Limited space

    Thanks

    Jim

  • In reply to Jim Perkins:

    Hi Jim,

    Thank you for the additional information.

    Assuming the DC motor is brushed, the following devices are also possible options:

    The DRV8847 which has:

     A voltage range of 2.7 to 18V
    Ability to monitor the current by adding an opamp on the external sense resistor
    RDSon of ~500mOhm in parallel (higher than the DRV8837)

     

    The DRV8850 which has:

     A voltage range of 2 to 5.5V ( 7V abs max -- this could be an issue)
    RDSon of 65mOhm
    Ability to monitor the current using the VPROPI output
    An integrated adjustable LDO that can provide up to 100mA

    Best Regards,
    Rick Duncan
    Motor Applications Team

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.