Hi Team,
I have an application where to enter lower power mode of my system, I disconnect VM and set it to 0V.
When I do this - I do not expect any current draw from the device except for leakage paths through the internal pull downs on nSleep, In1, and In2. Is that correct?
When VM =0V, I will have PMODE = 3.3V, IMODE = 0V, IPROPI =0V, and VREF = 3.3V. Will this damage the device? I believe it will not since the ABS MAX table shows these pins able to handle 5.75V independent of the supply. But I wanted to double check.
Thanks!
Reed