Other Parts Discussed in Thread: DRV8702-Q1,
For SPI communication between STM32F1 and DRV870x-Q1 chip, I am able to send the command data over MOSI but MISO line remains low during transfer and expected data is not received.
DRV870x-Q1 chip is enabled(not in sleep mode). None of the pins are shorted. Screenshot is for config register but behaviour is same for other reads also.
SPI configuration for STM master:
SPI mode: mode 0
First bit: MSB
Direction: full duplex
We tried different Baudrates 9MHz,4 MHz