Hello,
we are using the DRV8323RS Driver in several products and plattforms. To ensure a very low power consumation when electronic is turned off we also switch vm line of Driver while power Bridge and vdrain pin is supplied.
In some cases it happens that two high side Fets are turned on by Software and we switch of the vm line. I added a scope where you can see that vm line is slowly decreasing from 18V down to 10V (red line). Also I added the math function of gate voltage of high side by measuring gate voltage and substract the Phase voltage (blue line). Math result is shown in Purple line.
We see now that gate voltage also slowly decrease down to 2V Ugs until we make a disable of Driver.
Now our Question: Can any strange Situation happen in this Situation? we know from DRV8703 that VM must be in the same range than Vdrain. We checked datasheet of DRV8323 again but didn't find any Special Topic About.
Hope you can help us….