Hi everyone,
Recently i bought an evaluation board for controlling Brushless DC motor, the board is "DRV8350H-EVM".
i have programmed the microcontroller to spin a sensored motor of an electric bike, everything was ok, the motor was running with overcurrent cases : when i apply braking torque on the wheel or when i set suddenly the duty cycle to 0 in high speed.
after some hours of tests the board stopped working and a led red fault occurs.
would someone tell me how to clear this fault ?
thanks.