• Resolved

DRV8308EVM: Can i control motor programatically

Prodigy 10 points

Replies: 1

Views: 41

Part Number: DRV8308EVM

I purchased a DRV8308EVM driver but is it only control via the EVMDRV8308 software.

I wanna know what can I control the motor via UART or any communication method by programing? And TI had published any SDK to help that.

  • Hello,

    Thanks for posting on the MD forum!

    Unfortunately we do not have a way to do this. The EVM is designed to work with the PC via USB. 

    If possible you could use a USB/UART sniffer tool to copy the transactions coming from the PC or MCU but we do not have this to provide.

    Regards,

    -Adam