Hi,
I am currently doing board layout for a design which uses the DRV8353RS gate driver.
One thing that gets me a little confused, when digging through the part's datasheet, is the high-side gate current return path.
Looking at the layout guidelines (section 11.1) in the datasheet (quote): "...Minimize the loop length for the high-side and low-side gate drivers. The high-side loop is from the GHx pin of the device to the high-side power MOSFET gate, then follows the high-side MOSFET source back to the SHx pin. The low-side loop is from the GLx pin of the device to the low-side power MOSFET gate, then follows the low-side MOSFET source back to the SPx/SLx pins."
These recommendations on gate drive current loops seem pretty obvious for someone who has some experience with power electronics design and I totally agree concerning the low-side loop. I would also agree for the high-side loop if the DRV8353 would use "standard" bootstrap circuitry which is referenced to the according SHx pins. Now, what makes things a little confusing for me, is that the charge pump for the high-side driver supply is obviously referenced to VDRAIN (like it is shown in Figure 29). So, when a high-side FET is turned on, the necessary gate-charge is provided by a current which is drawn from the VCP capacitor (connected between VCP and VDRAIN). This means that the gate current flows out of the capacitor's VCP terminal - through the high-side driver - into the MOSFET gate - out of the MOSFET source - and where does it go now? Since the current needs to go back to the second terminal of the VCP capacitor, which is VDRAIN, there must be a path which allows the gate current to flow from SHx to VDRAIN. Looking at Figure 32 it don't see how this is achieved. I don't assume the current loop is closed through the high-side FET's body diode and the VDRAIN sense line - because that would be kind of awkward.
Since the gate drive current loop is a pretty critical topic, when it comes to board layout, I hope you can resolve my confusion.
Thanks and best regards,
Sebastian