Other Parts Discussed in Thread: DRV103, UCC28740, ISO1212
Hi I would like to use the DRV110 or DRV103 (with external power mosfet) to drive and AC 110/220 solenoid valve
The application note circuit are quite well explained but all schematic has NO galvanic insulation from the AC Load
Since the controller that drives the PWM current controller has some sensor, a GUI and buttons I'm little bit worried but a direct path to AC
Is there any way to insulate the AC part from the rest?
2nd question, what is the suggested frequency for a solenoid valve or linear actuator control via PWM ??
thanks
Davide