Hello team TI,
After long time i'm having conversation.
Sorry that i left last conversation incomplete. It is because i was shifted to another project.
Now i'm on Bldc ceiling fan project again.
My ceiling fan is perfectly rotating, but the issue is when fan is at maximum speed and if i make Duty to zero at the moment fan starts Jerk and then Coast smoothly.
Same thing happening when fan is already in rotating condition initially when Pwm=0 and then if i set fan speed maximum Pwm=100 motor jerk for the moment and then start rotation smoothly.
I've changed tuning parameter many times but could not solve this issue. And I'm running out of ideas.
DRV10983 parameter of EEPROM:
MotorParam1= 0x4C
0XCF
0X5E
0XC8
0XD0
0XFF
0X7F
0XE9
0X0F
0XFF
0XFF
SysOpt9 = 0X3E