Hi Adam,
I refer to my previous posts regarding DRV8320. I did a lot of tests with the driver (measure of Gate Source voltage at HS and LS, improve signal routing at the board, add addtional GS capacitor to improve dv/dt capability). At room temperature and above (up to 40°C) it worked fine. But now we did cold tests (-30...0°C) and now I saw the GDF again and the driver was again destroyed (next screenshot: channel 1 driver fault output, channel 2 phase current). Now I'm really unsatisfied and didn't have any idea what I can do to improve.
Do you have any suggestion what I can do? Addtional clamping or protection circuit?
BR
Martin