Other Parts Discussed in Thread: LAUNCHXL-F28027F, MOTORWARE
Hello
I have TI PN: BOOSTXL-DRV8305EVM with LAUNCHXL-F28027F.
I am using the above to drive a 3-phase BLDC sensorless motor (24V, 6.8A max) that runs a pump. Using the project solutions I have gotten the motor to run however the pump that the motor runs isn't turning on. The current draw is less than the nominal. I also notice that the referenced motor RPM is never reached. Which project lab can I fully operate the motor? Please advise.