Can I use ethernet on a blaze board which is running icecream sandwich Android?
Cheers,
Alireza
Hi Alireza,
Are you using Blaze board or Blaze Tablet? Please add "ip=dhcp" in your bootargs and check if it works.
Regards,Satheesh.
------------------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.------------------------------------------------------------------------------------------------------------------
Alireza,
Yes, Ethernet works on Blaze and Blaze Tablet with ICS, both with the built-in Ethernet port and with a USB-Ethernet gadget. (In the latter case, make sure to enable "USBNET" in your menuconfig.) As Satheesh mentioned, you can use "ip=dhcp" in the bootargs to have the IP address assigned. You could also use netcfg / ifconfig commands to assign a static IP address.
Regards,
Gina
Please click the Verify Answer button on this post if it answers your question
_______________________________________________________
Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ