• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » OMAP™ Applications Processors » OMAP 4 Forum » Getting OMAP Blaze up and running
Share
OMAP™ Applications Processors
  • Forums
Options
  • Subscribe via RSS

Forums

Getting OMAP Blaze up and running

This question is answered
Daniel Valencia
Posted by Daniel Valencia
on May 07 2012 15:14 PM
Prodigy30 points

Hello,

I found this link http://omappedia.com and it provides me with the pre-built binaries for Android. I do not have a Linux machine which is a requirement. I only have windows.

Is there any information on getting the Blaze running with WinCE? Or using windows?

Thank you

Daniel

blaze omap
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Venkat Ramana Peddigari
    Posted by Venkat Ramana Peddigari
    on May 08 2012 00:43 AM
    Expert4080 points

    Hi Daniel,

    Even if you do not have linux machine, another option is to install VmWare and set up Ubuntu on your windows PC to have the linux environment to download and build the code for Blaze.

    Thanks & Best Regards,

    Venkat

    Please click the Verify Answer button on this post if it answers your question
    _____________________________________________

    Be sure to read the OMAP4 Forum Guidelines & FAQ-

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Valencia
    Posted by Daniel Valencia
    on May 08 2012 08:45 AM
    Prodigy30 points

    Hello Venkat,

    Is there any step by step instructions on doing this? It sounds like this is an intermediate process. Is there anyway that I can just download the binaries on the SD card and plug it into the Blaze and then it would just run?

    Thanks for your help

    Daniel

    blaze
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Magdalena Iovescu
    Posted by Magdalena Iovescu
    on May 08 2012 13:25 PM
    Intellectual2480 points

    Hello Daniel,

    We have used Virtual Box in the past to run Linux on a Windows machine. Go to http://www.virtualbox.org/wiki/Downloads and download a version for your host OS. After you download it, you can install uBuntu (11.10 for instance) inside it. Internally at TI we have some reference Virtual Box images, but they are based on on uBuntu 10.04 and Windows XP.

    Regards,

    Magdalena

     

    Please click the Verify Answer button on this post if it answers your question

    _____________________________________________

    Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gina Glaser
    Posted by Gina Glaser
    on May 09 2012 07:57 AM
    Expert8055 points

    Daniel,

    I assume you want to run the Android pre-built binaries on your Blaze?  The issue is that your SD card has to be partitioned/formatted, and the binaries copied, in a very particular way in order for OMAP to be able to boot from the SD card.  This is done using a Linux PC (or Ubuntu running from VMWare).  I am not aware of an easy way to do this using a Windows PC.

    Regards,

    Gina

    Please click the Verify Answer button on this post if it answers your question

    _______________________________________________________

    Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Manuel Contreras
    Posted by Manuel Contreras
    on May 09 2012 17:04 PM
    Verified Answer
    Verified by Magdalena Iovescu
    Genius9115 points

    Daniel,

    You can try to use a Ubuntu LIVE DVD to do SD Card formating, (there are more Linux LIVE distributions to use, to compile Android FS it is sugested to use Ubuntu 64bits like indicated in http://omapedia.org/wiki/4AI.1.3_OMAP4_Icecream_Sandwich_Release_Notes)

    It is indicated to use Ubuntu 10.04, but Ubuntu 11.04 is working ok. it is recommended to use Google Chrome, Mozilla Firefox or a "download program" to download the DVD image.

    You can download this DVD iso image from (for mirror sites http://www.ubuntu.com/download/desktop/alternative-downloads)

    If you have a 64 Bits capable processor and/or plan to compile AFS download "...amd64.iso" image, if it is only to copy files to SD Card then use 32 Bits one "...i386.iso".

    you can find some options on how to burn the DVD and how to use a memory stick too,

    http://www.ubuntu.com/download/help/burn-a-cd-on-windows

    https://help.ubuntu.com/community/BurningIsoHowto

    http://www.ubuntu.com/download/help/create-a-usb-stick-on-windows

    then one time having the DVD ready put it in the DVD drive and restart your computer, check that CD/DVD drive boot is selected in BIOS, or if F12 options is enable press F12 and select CD/DVD drive as boot device, a menu window is going to give you many options if your plan is to run it in LIVE DVD select the first option,

    If you are planing to install it there are some precautions to take, this procedure modify your actual PC's hard drive configuration, easiest way is to look next link (check that your hard drive have enough space for the installation and manual installation see https://help.ubuntu.com/community/HowtoPartition)

    http://www.ubuntu.com/download/desktop/windows-installer

    always backup your information the first time if you plan a manual installation directly to the PC, read full post first.

    the better way for to try it is using VIrtualBox in this case if you make a mistake it will be restricted to virtual disc used, download necessary guest additions tools that improves performance of installed OS.

    the installation using VirtualBox is the same procedure than previously mentioned, DVD download, burn is not needed because VirtualBox can use either .iso or a burn image and HowtoPartition link and read VirtualBox user manual, Ubuntu installation is very friendly and more using graphic option.

    then follow SD Card formating instructions http://omappedia.org/wiki/Android_Build_SD_Configuration and respective Blaze release information http://omapedia.org/wiki/Release_Notes

    Please click the Verify Answer button on this post if it answers your question
    _______________________________________________________
    Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use