This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CUSTOM SRESP error with SOURCE:L4CFG when adding a *.so to my android HAL

 

Deal all,

            I encounter  the same  problem when I add a  *.so to my android HAL with blaze tablett2 omap4460 GP.

            Please help! 

            Thanks!

 [ 7.962432] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.966064] init: cannot find '/system/bin/arxd', disabling 'tiared'
[ 7.976287] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.983428] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 7.990325] omap_rpmsg_mbox_callback: received echo reply from ipu !
[ 8.080688] android_usb: already disabled
[ 8.088562] warning: `adbd' uses 32-bit capabilities (legacy support in use)
[ 8.096923] adb_open
[ 8.099700] mtp_bind_config
[ 8.103179] adb_bind_config
[ 8.106323] ------------[ cut here ]------------
[ 8.111480] WARNING: at arch/arm/mach-omap2/omap_l3_noc.c:135 l3_interrupt_handler+0x2e0/0x380()
[ 8.121246] CUSTOM SRESP error with SOURCE:L4CFG
[ 8.126373] Modules linked in:
[ 8.129882] Backtrace:
[ 8.132812] [<c005abcc>] (dump_backtrace+0x0/0x110) from [<c064a5d0>] (dump_stack+0x18/0x1c)
[ 8.142120] r6:00000087 r5:c0080804 r4:c7b319c0 r3:c7b30000
[ 8.148834] [<c064a5b8>] (dump_stack+0x0/0x1c) from [<c00a7884>] (warn_slowpath_common+0x5c/0x6c)
[ 8.158721] [<c00a7828>] (warn_slowpath_common+0x0/0x6c) from [<c00a7938>] (warn_slowpath_fmt+0x38/0x40)
[ 8.169189] r8:00000002 r7:f8000448 r6:00080003 r5:c0894ac0 r4:f8000400
[ 8.176818] r3:00000009
[ 8.179962] [<c00a7900>] (warn_slowpath_fmt+0x0/0x40) from [<c0080804>] (l3_interrupt_handler+0x2e0/0x380)
[ 8.190673] r3:c07b91c8 r2:c07b9164
[ 8.194854] [<c0080524>] (l3_interrupt_handler+0x0/0x380) from [<c00f4510>] (handle_irq_event_percpu+0x78/0x294)
[ 8.206146] [<c00f4498>] (handle_irq_event_percpu+0x0/0x294) from [<c00f4770>] (handle_irq_event+0x44/0x64)
[ 8.216979] [<c00f472c>] (handle_irq_event+0x0/0x64) from [<c00f6e04>] (handle_fasteoi_irq+0xa4/0x144)
[ 8.227325] r6:0000002a r5:c0867b8c r4:c0867b40 r3:c004e590
[ 8.234039] [<c00f6d60>] (handle_fasteoi_irq+0x0/0x144) from [<c00f4014>] (generic_handle_irq+0x40/0x48)
[ 8.244506] r5:c004f020 r4:c0876898
[ 8.248748] [<c00f3fd4>] (generic_handle_irq+0x0/0x48) from [<c0050060>] (asm_do_IRQ+0x60/0xc0)
[ 8.258361] [<c0050000>] (asm_do_IRQ+0x0/0xc0) from [<c064e508>] (__irq_svc+0x48/0xe0)
[ 8.267181] Exception stack(0xc7b31ab8 to 0xc7b31b00)
[ 8.272857] 1aa0: 00000103 c090f9a0
[ 8.281890] 1ac0: c090f9a0 00000000 00000202 00000000 c7b30000 c0866040 00000001 c090f9a0
[ 8.291015] 1ae0: 00000000 c7b31b4c c7b31b00 c7b31b00 c00afaf0 c00af620 20000113 ffffffff
[ 8.300109] r7:00000104 r6:0000002a r5:fa240100 r4:ffffffff
[ 8.306762] [<c00af5a4>] (__do_softirq+0x0/0x288) from [<c00afaf0>] (irq_exit+0xb8/0xbc)
[ 8.315765] [<c00afa38>] (irq_exit+0x0/0xbc) from [<c005c100>] (ipi_timer+0x44/0x48)
[ 8.324401] r4:c004e040 r3:00000001
[ 8.328582] [<c005c0bc>] (ipi_timer+0x0/0x48) from [<c005045c>] (do_local_timer+0x68/0x84)
[ 8.337768] r5:c004f020 r4:c0876898
[ 8.341949] [<c00503f4>] (do_local_timer+0x0/0x84) from [<c064e508>] (__irq_svc+0x48/0xe0)
[ 8.351165] Exception stack(0xc7b31ba0 to 0xc7b31be8)
[ 8.356781] 1ba0: 60000113 00000002 c08adb38 00000000 c08ef578 00000003 c08ada90 c08ef58b
[ 8.365875] 1bc0: 00000025 00000000 00000000 c7b31c9c c7b31bb8 c7b31be8 c00a864c c00a8e4c
[ 8.374969] 1be0: 60000113 ffffffff
[ 8.378875] r7:00000002 r6:0000001d r5:fa240100 r4:ffffffff
[ 8.385589] [<c00a89e4>] (vprintk+0x0/0x5ec) from [<c064a7b4>] (printk+0x24/0x2c)
[ 8.393859] [<c064a790>] (printk+0x0/0x2c) from [<c03c580c>] (adb_function_bind_config+0x28/0x94)
[ 8.403717] r3:c0955b84 r2:c03c57e4 r1:c08c8da8 r0:c07fcf54
[ 8.410369] [<c03c57e4>] (adb_function_bind_config+0x0/0x94) from [<c03c58b8>] (android_bind_config+0x40/0x7c)
[ 8.421478] r5:c08c8ed0 r4:00000000
[ 8.425720] [<c03c5878>] (android_bind_config+0x0/0x7c) from [<c03c4b94>] (usb_add_config+0xac/0x124)
[ 8.435913] r7:00000000 r6:c03c5878 r5:c7b5cd80 r4:c08c8da8
[ 8.442626] [<c03c4ae8>] (usb_add_config+0x0/0x124) from [<c03c7848>] (android_enable+0x4c/0x90)
[ 8.452392] r7:c7b5ccc0 r6:c7b5ef80 r5:00000001 r4:c7b5cd80
[ 8.459045] [<c03c77fc>] (android_enable+0x0/0x90) from [<c03cc6a0>] (adb_open+0xcc/0xd0)
[ 8.468139] r4:c7b5ccdc r3:00000001
[ 8.472320] [<c03cc5d4>] (adb_open+0x0/0xd0) from [<c031f4a4>] (misc_open+0x23c/0x4a4)
[ 8.481140] r7:c08bf094 r6:c78c3d80 r5:00000037 r4:c0682ddc
[ 8.487854] [<c031f268>] (misc_open+0x0/0x4a4) from [<c01563c8>] (chrdev_open+0x13c/0x270)
[ 8.497009] [<c015628c>] (chrdev_open+0x0/0x270) from [<c0150f20>] (__dentry_open+0x198/0x348)
[ 8.506591] [<c0150d88>] (__dentry_open+0x0/0x348) from [<c01511b0>] (nameidata_to_filp+0x68/0x70)
[ 8.516540] [<c0151148>] (nameidata_to_filp+0x0/0x70) from [<c015fd70>] (do_last+0xc8/0x6d8)
[ 8.525939] r7:00000026 r6:00000000 r5:00020002 r4:c7b31ed0
[ 8.532592] [<c015fca8>] (do_last+0x0/0x6d8) from [<c01613b8>] (path_openat+0xc4/0x3d4)
[ 8.541503] [<c01612f4>] (path_openat+0x0/0x3d4) from [<c01617c0>] (do_filp_open+0x38/0x8c)
[ 8.550811] [<c0161788>] (do_filp_open+0x0/0x8c) from [<c0150c9c>] (do_sys_open+0xe8/0x17c)
[ 8.560028] r8:00000001 r7:ffffff9c r6:00000008 r5:00020002 r4:c6d04000
[ 8.567993] [<c0150bb4>] (do_sys_open+0x0/0x17c) from [<c0150d68>] (sys_open+0x24/0x28)
[ 8.576904] [<c0150d44>] (sys_open+0x0/0x28) from [<c00568a0>] (ret_fast_syscall+0x0/0x30)
[ 8.586029] ---[ end trace cf914694fb5ef19e ]---
[ 8.591247] Master 0x44 DucatiM3
[ 8.595031] L4CFG OPCODE 0x00000002
[ 8.599151] ------------[ cut here ]------------
[ 8.604309] WARNING: at arch/arm/mach-omap2/omap_l3_noc.c:135 l3_interrupt_handler+0x2e0/0x380()
[ 8.613952] CUSTOM SRESP error with SOURCE:L4CFG
[ 8.619049] Modules linked in:

 

 

 

  • Zhang,

    You mentioned: "I encounter  the same  problem when I add a  *.so to my android HAL with blaze tablett2 omap4460 GP."

    Can you please explain specifically what you changed/added?  Do you mean that you never have the issue ("CUSTOM SRESP error with SOURCE:L4CFG") before making this change, and you always have the issue after making this change?

    Thank you,
    Gina 

    Please click the Verify Answer button on this post if it answers your question

    _______________________________________________________

    Be sure to read the OMAP4 and OMAP5 Forum Guidelines and FAQ 

  • In reply to Gina Glaser:

    Hi,Gina

            Thank you for your reply!

            The issue resulted from my  *.so. Now , I have solved the problem.

            Thank you again!

     

     

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.