This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

use 8 megapixel camera on omap4460

I use 8 megapixel camera OV8825 on OMAP4460 and modified ducati imx_060 for using OV8825.Now can work on preivew and record mode, but can not work on capture mode. Any idea?

OV8825 is a RAW RGB 10-bit(BGGR) camera.The ducati debug messages are below:

[ 1.765] [ERR=2625] src/new_sensor_MSP.c:[534]:Sen Read ID: 34853, expected ID:34853
[ 1.765]
[ 1.765] [ERR=2626] OV8825/src/OV8825.c:[1104]:!!! Sensor active!

[ 1.834] [ERR=4355] OV8825/src/OV8825.c:[1232]:Set Sensor configuration:SEN_MODE_PREVIEW
[ 1.835] [ERR=4356] src/msp_camera_api.c:[1462]:COLOR Pattern: 2
[ 1.835]
[ 1.835] [ERR=4357] src/new_csi_MSP.c:[450]:Default complex IO configuration for CSI:0
[ 1.835] [ERR=4358] src/csi2rx_api.c:[502]:number = 0, imagebuf = @b49000a0
[ 1.835] [ERR=4359] src/new_csi_MSP.c:[450]:Default complex IO configuration for CSI:0
[ 1.835] [ERR=4360] src/csi2rx_api.c:[502]:number = 1, imagebuf = @b5c38ea0
[ 1.836] [ERR=4369] src/face_detect_alg_integration_module.c:[759]:initFaceDetectPrivateContext: Loading DCC parameters for face detect failed. Loading default values.
[ 1.837] [ERR=4376] src/hal_manager.c:[579]:hai_manager_config_camera: HAL Camera configuring... (Compile Time: Nov 21 2011 19:46:13)
[ 1.843] [ERR=4378] src/awb_fw.c:[914]:auto_white_balance_create: AWBFW : AWB DCC ERRORS. DUMMY TUNNING LOADED.
[ 1.848] [ERR=4381] source/af_fw_dcc.c:[195]:affw_parse_dcc_content: AFFW : Invalid AF DCC server data! Use Defaults!
[ 1.849] [ERR=4382] source/af_fw_dcc.c:[217]:affw_parse_dcc_content: AFFW : Invalid HLLC DCC server data!
[ 1.849] [ERR=4383] source/af_fw_dcc.c:[239]:affw_parse_dcc_content: AFFW : Invalid AFFW DCC server data!
[ 1.849] [ERR=4384] source/af_fw_dcc.c:[264]:affw_parse_dcc_content: AFFW : Invalid CAF DCC server data!
[ 1.859] [ERR=4385] src/eeprom_lib.c:[521]:eeprom_lib_sensetivity_array: EEPROM:NULL pointer magic X 57005
[ 1.943] serviceMgr: received msg type: 4 from addr: 1025
[ 1.944] serviceMgr: OMX_DISCONNECT: len 4, addr: 101
[ 1.944] RcmServer_serverThrFxn_P: Exiting thread.
[ 1.944] deleteService: removed RcmServer at endpoint: 101

[ 50.808] [ERR=70922] src/hal_manager.c:[579]:hai_manager_config_camera: HAL Camera configuring... (Compile Time: Nov 21 2011 19:46:13)
[ 50.814] [ERR=70923] src/awb_fw.c:[914]:auto_white_balance_create: AWBFW : AWB DCC ERRORS. DUMMY TUNNING LOADED.
[ 50.821] [ERR=70927] src/msp_camera_api.c:[3367]:NO Camera FLASH module
[ 50.821]
[ 50.821] [ERR=70934] OV8825/src/OV8825.c:[1211]:Set Sensor configuration:SEN_MODE_CAPTURE
[ 50.822] [ERR=70977] dspbios/kgenerator/kg_preflash.c:[185]:kg_preflash_required: ERROR: Disable PREFLASH sequence because HARDWARE missing
[ 50.824] [ERR=70990] src/eeprom_lib.c:[521]:eeprom_lib_sensetivity_array: EEPROM:NULL pointer magic X 57005
[ 50.827] [ERR=70998] src/new_csi_MSP.c:[450]:Default complex IO configuration for CSI:0
[ 50.827] [ERR=70999] src/csi2rx_api.c:[502]:number = 0, imagebuf = @00000000

  • In reply to Ray Tang:

    By the way,how to use ducati ISS ISP H3A function for camera?

  • In reply to Ray Tang:

    That functionality is already implemented in Ducati framework. You don't need to do anything extra. Just get your sensor running and 3A will be working automatically.

    You will need to tune 3A for optimum image quality, but that is a different topic all together.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.