Dear,
From the TRM of OMAP4460,we know that the CPI of it is 16-bit wide, BT656 and SYNC mode.
Is 16-bit YUV format supported by it ?for example,may I connect output of TVP7002(16bit YUV) to it?
As the TRM says - in sync mode no assumption is made about pixel format. Therefore 16-bit mode can be used to transfer YUV data.
------------------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question. ------------------------------------------------------------------------------------------------------------------
Does it really possible?
if http://e2e.ti.com/support/omap/f/849/p/239265/842710.aspx#842710
we can'nt do this, who can?
Does it make work by anybody?