I am using a 10.1" 1360x768 Active or TFT 18bit LCD display, which is connected over LVDS. Lot of artigraft is visible in the LCD output and no change in output after enabling the different Dithering mode. As it is LCD in TFT mode, when I enable the Dithering mode, the STN Dither logic and output FIFO bypassed.
How to achieve the Dithering in OMAP4? If I change the LCD to STN mode, it is not working and no output on the screen.