Hi all,
I just started working on a project that need the use of two cameras that acquire in the same time two different images like is usually done in the 3d systems but this is not my case. I would like to have some information about the best way to cononect 2 cameras to omap4 and the capability of the linux camera driver to manage to different cameras simultanously.
My project is in an early stage and for now i can imagine two possibility:
1) Use two USB camera connected to the processor. Omap4 is powerful enough to manage two 3.1Mpix camera on linux?
2) I have to create a dedicated board, so i can mount directly two cmos (the right one with linux driver aptina or OV) on the board and connect them to CSIA and CSIC
In the second case linux can recognize the cameras as two different devices? You know some reference design or existing project that can aid me in this way?
Thanks in advance,
Giulio