Hi,
I am in process of integrating the TLV320AIC3104 with omap4460, and I have done the necessary machine driver changes.
When I play a file through tinyplay command , I am not able to see the Data coming into the codec DIN pin through probing and
cat /proc/asound/card0/pcm0p/sub0/status not showing proper hw_ptr increments, and audio is not heard on the speaker.
I am suspecting the clock are not supplied properly. The clock that I feed are as follows.
MCLK - 19.2MHZ
BCLK - 24MHZ
WCLK- 12KHZ.
Do see any problem in the above clock values?
I am configuring MCBSP as master and codec as slave.
Any help on this is highly appreciated.
Kind Regards,
Sandeep S.P