I have two questions.
1) I want to put McBSP1 in master mode. When doing that I want to SRG to run off McBSP1_ICLK. What is the register setting for that? and what is the clock rate of McBSP1_ICLK?
2) The machine driver calls snd_soc_set_sysclk(X, X, 64*param_rate(params), X, X). The interface is running at 8 kHz. Why is the multiple of 64 there? If my set up is
FS = 8 kHz, 1 channel and word length of 16 bit what should this value be?