In order to learn about TI RTOS and my C6000 Microcontroller I have been going through the labs and lessons for the TI RTOS Kernal Workshop. I got to lesson 4 using TI-RTOS and the first half of it went really well until I went to add in the UIA services to enable a lot of the debugging features. When I did this I could still compile but when luanching in the debugger the code always started and was stuck in "exit.c" under "_CODE_ACCESS void abort(void)" function and my blink LED no longer worked or ran. Any idea what got messed up here when I added int he UIA or what I need to adjust?
Versions:
XDC (3.25.02.70)
BIOS(6.35.03.47)
UIA(1.03.01.08)
CCS V6
OMAP L138 LCDK