OMAP 4430 GPMC Burst mode
Hi all,
Im working on OMAP 4430, and I have it connected to a Cyclone 5 FPGA through the GPMC bus. I would like to use burst mode. I configured the OMAP GPMC registers to use burst mode:
0x78001200 //GPMC_CONFIG1_i
0x00131300 //GPMC_CONFIG2_i
0x00030300 //GPMC_CONFIG3_i
0x13041308 //GPMC_CONFIG4_i
0x00111313 //GPMC_CONFIG5_i
0x840404c4 //GPMC_CONFIG6_i
Is there anything else I need to configure to get the burst mode working? Does the clock speed matter?
I expect the chip select to stay low through all the reads/writes, but currently is toggling back and forth with each read/write.
I have read on other posts, that others have configured their DMA to get the burst mode working, is this a necessary step to get the burst mode?
Thanks,
Christian Archilla