Hi,
I am currently implementing a driver to capture video from the OMAP4460's CPI port. The input is a BT.656 (YUV422 8bit) interlaced video stream.
According to the OMAP4460 TRM, section 8.2.2.3.2, Figure 8-10, it appears that the video signals containing a BT.656 stream should be connected to the ISS on cam2_d[11:4] and not cam2_d[7:0]. I did not find any text to back this up, though...
1. Do I need some special setting to tell the ISS to take data from [11:4] instead of [7:0] ? or is this implicit when enabling BT.656 from register ISIF_REC656IF.
2. I am also unsure as to how I tell the ISS/ISIF how many bytes per line I have considering the fact that the data input is the VPORT (IPIPEIF_CFG1.INPSRC1=0 and IPIPEIF_CFG1.INPSRC2=0)
Any help would be greatly appreciated...
Thanks,
Marc