I am using RaccoonBoard Development Kit.
I used software release here: http://59.124.231.13/index.php/JAJ_2.5-P2_AP_Module_OMAP4_Jelly_Bean_Release_Notes
I encounted a problem that is "Unable to handle kernel paging request at virtual address 86000000" when internet traffic increase.
I've googled and saw that the issue caused because Memory fragmentation
And SLUB allocator can reduce Memory fragmentation, so I want to change to it
I use "make menuconfig" to enable SLUB and disable SLAB
But my board can't boot, At console windows, I see following log error run continually:
[ 12.792724] init: untracked pid 106 exited
[ 13.528839] init: untracked pid 431 exited
[ 18.054626] init: untracked pid 432 exited
[ 20.428802] init: untracked pid 436 exited
[ 23.597076] init: untracked pid 437 exited
[ 28.877624] init: untracked pid 443 exited
[ 34.060852] init: untracked pid 451 exited
[ 34.174468] init: untracked pid 457 exited
[ 39.325408] init: untracked pid 470 exited
[ 39.440093] init: untracked pid 476 exited
[ 44.604644] init: untracked pid 489 exited
[ 44.760406] init: untracked pid 495 exited
[ 49.875366] init: untracked pid 508 exited
[ 50.002563] init: untracked pid 514 exited
Anybody know about this issue, please help me
Regards,
Anh