I already write ubuntu 12.04 in SD card ,
and I plug SD card in pandaboard.
and open minicom
but I don't know why minicom resend this message .
Could you answer me?
THX
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I already write ubuntu 12.04 in SD card ,
and I plug SD card in pandaboard.
and open minicom
but I don't know why minicom resend this message .
Could you answer me?
THX
Hi,
This is because your u-boot does not properly initializes the sdram (see sdram-init() function in u-boot/arch/arm/cpu/armv7/omap-common/emif-common.c). You've probably built your u-boot with the wrong configuration file.
Could you please share, which release are you using? Official releases for pandaboard can be found here: http://www.omappedia.org/wiki/Ubuntu_Pre-Built_Binaries
Best Regards,
Yordan
I think that I did not install u-boot Completely.
so could you send complete SOP flow to me for omap4460 pandaboard ES Ver.B3 ?
I download from this path:git clone git://git.omapzoom.org/repo/u-boot.git
I find out the someone SOP .
but I think that it is not for my pandaboard
-----------------------------------------------------------------------------------------------
cd $PANDA_WORK
git clone git://git.omapzoom.org/repo/u-boot.git
cd u-boot
git checkout -b omap4_dev origin/omap4_dev
wget http://android-development-environment.googlecode.com/files/0001-change-bootarges.patch
git apply 0001-change-bootarges.patch
make omap4430panda_config
make -j8
cp -a u-boot.bin $ANDROID_ROOT/device/ti/panda/bootloader.bin
by the way,I already install ubuntu 12.04 from pre-built binary,
the install file:http://cdimage.ubuntu.com/releases/12.04/release/ubuntu-12.04-preinstalled-desktop-armhf+omap4.img.gz
so I think that I don't have the question of boot.
THX
Is it possible that I hava other queestions?