Hi,
I'm not sure if this is the right place to ask about this, but I think I burned my Pandaboard ES. I accidentally plugged a 12V power supply, the red overvoltage indicator light up, but now it doesn't seem to boot. Only one of the green leds lights up.
It was my first attempt to run it, so I'm not 100% sure if I'm doing it right though. I plug a 5v usb power, the adaptor is capable of supplying 2A.
Does that only 1 led lighting means that the board is gone? Is there any way I could try to repair it - resolder some stuff, etc?
Btw can it be powered from the usb connector? Could this be the problem - that I don't use a mains power supply?
Thanks!