hello,
I got some error messages when I use command mode.
omapdss DSI error: DSI CIO error, cio irqstatus 200000
omapdss DSI error: Failed to complete previous l4 transfer
omapdss DSI error: vc(0) busy when trying to config for VP
omapdss DSI error: TE not received for 250ms!
omapdss DSI error: Framedone not received for 250ms!
Could you help me to solve this error?
Which setting or code do I need to build in source code?
I just want to send LCD module initial code(OK) and frame data( not OK ; OS give).
And I find out that dsi_update_screen_dispc's datas are zeros.
Including w, h, bytespp, bytespl, bytespf, total_len, packet_payload, packet_len.
PS: bytespp = dssdev->ctrl.pixel_size / 8; this code doesn't work. WHY?