Hi,
I try to re-flash eMMC, after powering on the uEVM board, the Host still display "waiting for device...", looks nothing happens. I have already flashed once. I'd like to know how to flash new image file to eMMC.
Thanks!
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi John , commonly this is due to the wrong version of usbboot for the release you are working with. Can you give more information, for your revision and software version you are trying to flash
Hi Boyko,
Thanks for your response!
I tried to usbboot -v(or --version), it did not work. I don't know how to check the version. however, I just downloaded from TI website yesterday. my board is uevm5432g-02-12-00.
I also tried the usbboot of re-building from source code.
John
Are you able to open debug session with the debug usb, if yes
replace your usbboot file with this one. and execute " sudo usbboot -f "
(it is for es1.0)
hope this helps
Hi Boyko,
Thank you very much!
How do i open debug session with the debug usb? i just replaced the usbboot and ran the "sudo ./usbboot -f", looks it same like before, the uEVM automatically enters android.
John Liu
As described in http://omapedia.org/wiki/Panda5AJ.1.3_Release_Notes
you set all the dip switches to OFF state, plug your your micro usb cable into the debug port, and execute :
sudo screen /dev/ttyUSB0 115200
note: be sure to monitor the correct ttyUSB number
after that you run usbboot and you power on the device.
Hi Boyko,
Thank for your help!
I think I figured out the problem, the usbboot has bug for USB3.0, the ENDPOINT descriptor of usb2.0 is 7 bytes, it is added companion part in USB3.0. the usbboot still uses the usb2 structure, so it only works on USB 1.0 & USB2.0, not for USB3.0.
John
Hi,
Iam new to omap platform. I received OMAP5432uEVM ES2.0 board. I followed the steps mentioned in
http://omapedia.org/wiki/Panda5AJ.1.4_Release_Notes. Using pre-built images, iam unable to boot the board.
when i tried giving the command from VM ubuntu/VBox ubuntu as
sudo ./usbboot -f. Ima getting the following error ""
Hi,
Iam new to omap platform. I received OMAP5432uEVM ES2.0 board. I followed the steps mentioned in
http://omapedia.org/wiki/Panda5AJ.1.4_Release_Notes. Using pre-built images, iam unable to boot the board.
when i tried giving the command from VM ubuntu/VBox ubuntu as
sudo ./usbboot -f. Ima getting the following error "sudo: unable to execute ./usbboot: No such file or directory".
I even tried with sd boot, still unsuccessful..
kindly help how to proceed further
BR
SKumar
Hi SKumar,
Did you make it executable (sudo chmod +x usbboot)?
Regards,
Boyko
Hi Bokyo,
Thanks for your reply.
I gave executable permissions too. Following error is diplayed.
sudo: unable to execute ./usbboot: No such file or directory"
I tried with VMWare and VBox with ubuntu 13.10 as host. But still not successful.
Even with SD card there is no success.
BR,
Skumar
Hi Skumar,
If you're trying to run a 32-bit binary on an amd64 installation:
-Up to Ubuntu 11.04, install the package ia32-libs.
-On Ubuntu 11.10, install ia32-libs-multiarch.
-Starting with 12.04, install ia32-libs-multiarch, or select a reasonable set of :i386 packages in addition to the :amd64 packages.
Regards,
Boyko
Hi,
The steps has been solved after installing ia32libs. Now the following error message is like this
sudo ./usbboot -f
Itwaiting for device...
The same message is from almost 3o minutes and no progress further.
i get information of lsusb . In VM usb setting is 3.0.
####################################
Bus 001 Device 007: ID 0403:6010 Future Technology Devices International, Ltd FT2232C Dual USB-UART/FIFO IC
Bus 001 Device 002: ID 80ee:0021 VirtualBox USB Tablet
Bus 001 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
#####################################
I followed the below thread too
http://e2e.ti.com/support/omap/f/885/p/322615/1124654.aspx#1124654
still unsuccessful.
Regards,
Suresh Kumar
Its not resolved even after pressing reset. Iam trying in Virtualbox with ubuntu 13.10 as host.
No error logs from minicom port also.
USB3 cable was not detected in my pc environment. I verified with colleague's environment and its working fine.