Hello all,
While using the omap5432evm we've encountered some issues that we haven't been able to solve.
Were using the 5AJ1.5.1 software found on the ti site.
Android version 4.2.2
linux kernel 3.4.48
Does anyone now how to fix the following issues:
- Command mode using the panel-taal.c driver has a slight delay. Video mode works perfectly so its not panel related. Is there a fix for this or a panel driver that works properly?
-USB doesn’t start always if not doing a cold start. When failing the following error repeats several times
ehci-omap echi-omap.0: port 2 reset error -110
- Terminal goes into some kind of sleep mode if no input is given and the first key entered after that will be ignored.
- When mounting an usb through the terminal the contents of this usb cannot be seen through a file viewer in android. This is probably because I dont have root access when using android through the android GUI. Is there a way to fix this without rebuilding android?
Any help would be appreciated.
Best regards,
Anthony