I am seeing following kernel backtrace on J6 with linux 3.8.13 when trying to start IVI LayerManager service. Before starting LM, I started the X11 and run some GLES2/X11 based tests successfully.
[ 719.005340] BUG: spinlock lockup suspected on CPU#0, kworker/u:2/787
[ 719.011749] lock: sync_lock+0x0/0x20, .magic: dead4ead, .owner: kworker/u:2/787, .owner_cpu: 0
[ 719.020507] [<c001bbc0>] (unwind_backtrace+0x0/0x138) from [<c02896d0>] (do_raw_spin_lock+0x100/0x17c)
[ 719.029876] [<c02896d0>] (do_raw_spin_lock+0x100/0x17c) from [<c03157ec>] (omap_gem_set_sync_object+0x14/0xf4)
[ 719.039978] [<c03157ec>] (omap_gem_set_sync_object+0x14/0xf4) from [<bf0091f4>] (FreeMemCallBackCommon+0xf4/0x24c [omapdrm_pvr])
[ 719.051635] [<bf0091f4>] (FreeMemCallBackCommon+0xf4/0x24c [omapdrm_pvr]) from [<bf0093d0>] (UnwrapExtMemoryCallBack+0x28/0x68 [omapdrm_pvr])
[ 719.064544] [<bf0093d0>] (UnwrapExtMemoryCallBack+0x28/0x68 [omapdrm_pvr]) from [<bf013d3c>] (FreeResourceByPtr.part.0+0xac/0xcc [omapdrm_pvr])
[ 719.077575] [<bf013d3c>] (FreeResourceByPtr.part.0+0xac/0xcc [omapdrm_pvr]) from [<bf0144d0>] (ResManFreeResByPtr+0x44/0x6c [omapdrm_pvr])
[ 719.090118] [<bf0144d0>] (ResManFreeResByPtr+0x44/0x6c [omapdrm_pvr]) from [<bf008980>] (async_unmap+0x28/0x44 [omapdrm_pvr])
[ 719.101531] [<bf008980>] (async_unmap+0x28/0x44 [omapdrm_pvr]) from [<c0315528>] (sync_op_update+0x88/0xa8)
[ 719.111328] [<c0315528>] (sync_op_update+0x88/0xa8) from [<c03157c8>] (omap_gem_op_update+0x14/0x24)
[ 719.120544] [<c03157c8>] (omap_gem_op_update+0x14/0x24) from [<bf010578>] (PVRSRVMISR+0xc/0x60 [omapdrm_pvr])
[ 719.130523] [<bf010578>] (PVRSRVMISR+0xc/0x60 [omapdrm_pvr]) from [<c005a810>] (process_one_work+0x1c8/0x5c0)
[ 719.140502] [<c005a810>] (process_one_work+0x1c8/0x5c0) from [<c005af58>] (worker_thread+0x168/0x444)
[ 719.149810] [<c005af58>] (worker_thread+0x168/0x444) from [<c005fa40>] (kthread+0xa4/0xb0)
[ 719.158142] [<c005fa40>] (kthread+0xa4/0xb0) from [<c00140d0>] (ret_from_fork+0x14/0x24)
Vikas