Hi,
I am trying to run Linux on the board using an sd card.
When I boot the board I get the following ( and no more output after 'Starting kernel').
U-Boot SPL 2013.01-gdc6238c (Mar 27 2013 - 14:33:47)
OMAP5432 ES2.0
die_id1: 15d6074
lisa_map_2: 0x80740300
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01-gdc6238c (Mar 27 2013 - 14:33:47)
CPU : OMAP5432 ES2.0
Board: OMAP5430 EVM
I2C: ready
DRAM: 2 GiB
relocation Offset is: 7e101000
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
In: serial
Out: serial
Err: serial
Hit any key to stop autoboot: 0
reading omap5-uevm.dtb
42953 bytes read in 11 ms (3.7 MiB/s)
reading uImage
4466736 bytes read in 287 ms (14.8 MiB/s)
## Booting kernel from Legacy Image at 80300000 ...
Image Name: Linux-3.13.0-rc7-g692ddae
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4466672 Bytes = 4.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 825f0000
Booting using the fdt blob at 0x825f0000
Loading Kernel Image ... OK
OK
Loading Device Tree to feef2000, end feeff7c8 ... OK
Starting kernel ...
If anyone knows what's the problem.
Thanks