Hello,
When I try to verify omap5432 USB gadget driver, I get an error:
ERROR: could not insert 'g_zero': No such device
I compare "USB3.0 device (gadget) mode support on linux SDK" description with my setting; but I can't get proper result.
my verifying condition:
Hardware EVM: OMAP5432 ES2.0
Software platfore: ti-glsdk_omap5-uevm_6_03_00_01
Test gadget modules: g_zero and g_mass_storage
The UsbGadget.config is the configuration of USB gadget.
To disable, enable DWC3 to DUAL or gadget only are the same result.