Hi experts,
I might do wrong instructions, so I describe how I did validation on the board:
1. connect directly J2 and J3 (H-H, L-L), and leave J1 no-POP
2. canconfig can0/1 bitrate 50000 ctrlmode triple-sampling on
3. ip link set can0/1 up
These process are OK, and we can see interrupts as well.
4. cansend can0 -i 0x10 0x11 0x22 0x33 0x44 0x55 0x66 0x77 0x88
5. candump can1
Nothing
The weird thing is the interrupt counter of can0 will always increase, even if I remove the connection between J2 and J3.
kernel version and commit id are the following:
3.8.13
commit 7c7bc6be666f87c9c9d4e2f47dfb52180cf01c8c
Merge: 71a6fd5 6b70f21
Author: Somnath Mukherjee <somnath@ti.com>
Date: Fri Jul 11 17:43:44 2014 +0530