Hi,
I have Vayu Evm xc5777x CPU board(DRA7XX).
I am trying to use ssh for gdb debugging using ccs 5.5.
I have successfully able to build and port the ssh on the board .
For this I am using the source code of the following packages:
1. zlib-1.2.7 .
2. openssl-1.0.0c .
3. openssh-6.6p1 .
After that I am using the following steps to compile them:
Build Zlib:
cd zlib-1.2.7
CC=arm-linux-gnueabihf-
./configure --prefix=$HOME/zlibArm
make
make install
Build OpenSSL:
export cross=arm-linux-gnueabihf-
cd openssl-1.0.0c
./Configure dist --prefix=$HOME/opensslArm
make CC="${cross}gcc" AR="${cross}ar r" RANLIB="${cross}ranlib"
make install
Build OpenSSH:
./configure --prefix=$($PWD) CC=arm-linux-gnueabihf-gcc AR=arm-linux-gnueabihf-ar --host=arm --with-libs \
--with-zlib=/home/mistral/zlibArm \ --with-ssl-dir=/home/mistral/opensslArm --disable-strip -- prefix=/home/mistral/Downloads/openssh-6.6p1/build/bin
make
make install
After that I put all the required files on the board .
Also I have uncomment the Port 22 in file /etc/sshd_config file.
root@dra7xx-evm:~# ssh
usage: ssh [-1246AaCfgKkMNnqsTtVvXxYy] [-b bind_address] [-c cipher_spec]
[-D [bind_address:]port] [-E log_file] [-e escape_char]
[-F configfile] [-I pkcs11] [-i identity_file]
[-L [bind_address:]port:host:hostport] [-l login_name] [-m mac_spec]
[-O ctl_cmd] [-o option] [-p port]
[-Q cipher | cipher-auth | mac | kex | key]
[-R [bind_address:]port:host:hostport] [-S ctl_path] [-W host:port]
[-w local_tun[:remote_tun]] [user@]hostname [command]
But I am getting an error.
ssh: connect to host 192.168.13.21 port 22: Connection refused
Please help in this regards
Regards
Naveen Sheeti