Hi Experts,
I am trying to get UYVY data from resizer, But form first frame it is dumping with all zero and for second exited with timeout.
Let me explain certain things for better understanding the issue.....
1> working on OMAP5 uEVM with ti-glsdk_omap5-uevm_6_04_00_02 package.
1> I am able to get the RAW data from sensor for "SENSOR -> CSI2A -> MEMORY" path.
2> And also I am able get the RAW data for "SENSOR -> VP -> IPIPEIF -> ISIF -> MEMORY" path
But the finally I need to capture 422 UYVY data from resizer by using V4L2 image capture application. So for this I configured the path as...
"SENSOR -> VP -> IPIPEIF -> ISIF -> IFIPEIF -> IPIPE -> RSZ -> BL -> SDRAM"
In this case only basic core modules are enabled to convert raw data yuv in IPIPE and resizer is also in pass through mode.
Issue is I am not able run my capture application for more than 1 frame, exited with timeout error and first frame data is also zero's
Can you help me to fix this issue ?
Thanks in Advance :)
Regards,
Gajanan