Hi,
I have an application that uses the hardware decoding functionality of OMAP5. This application is currently using DCE 3. I've compiled DCE 4 and i'm trying to replace DCE 3 with DCE 4 in my application, but i got the following error:
MmRpc_call: Error: write failed -1
The code that fails is the following:
/* send message for remote execution */
status = write(obj->fd, msg, len);
if (status < 0) {
printf("MmRpc_call: Error: write failed %d\n", status);
status = MmRpc_E_FAIL;
goto leave;
}
I get this error in VIDDEC3_process.
Thank you,
Alexandra