Hi,
I'm using OMAP57xx processor on DRA7xx EVM. I've built Linux file system and booted the board from SD card. I compiled one application for ARM and loaded into the Linux file system and it's running fine. Now I need to build and run an application for DSP. How can I build the application for C66x cores? How to run it? Can I run the DSP application after booting board from SD card with Linux?