My customer made a mistake on their board layout, and crossed DDR1_A15 and DDR1_A14 at the DRAM. Due to the board layout, they can’t cut the trace at the DRAM. The best option that we see is to drill the via at the processor for A15 and connect A14 to the termination resistor. At this point, it will leave about a 1” stub. Not good, but might work.
Another option that we wanted to explore is if the A15 and A14 lines can be turned off via the PINMUX. There is no listed PINMUX for these pins, but we're hoping something can be done that is undocumented. The datasheet mentions most pads are set to MUXMODE 0xF by default, which is HI-Z, but it's not clear if that's the case for DDR pins.
The question that we really want to find out is if we can turn off the driver for DDR1_A15 via software while enabling the rest of the DDR1 interface. If so, how is it done?
Thanks,
David