Hi,
I need to vary the cpu frequency so I am trying to install omapconf on my OMAP 5432 board which has Ubuntu 12.04.5 LTS installed on it.
First I tried:
root@localhost:~# sudo apt-get install tiomapconf
and got the following result:
Reading package lists... Done
Building dependency tree
Reading state information... Done
E: Unable to locate package tiomapconf
Later I tried the following instructions:
1. cloned sources from github: https://github.com/omapconf/omapconf.git
2. # cd ~/omapconf/omapconf
3. #export PATH=/home/bin/toolchains/arm-2010q1/bin/:$PATH
4.#make CROSS_COMPILE=arm-none-linux-gnueabi- omapconf
and led to the following:
root@localhost:~/omapconf-master# make CROSS_COMPILE=arm-none-linux-gnueabi- omapconf
make: arm-none-linux-gnueabi-gcc: Command not found
make: Warning: File `omapconf.c' has modification time 1.4e+09 s in the future
arm-none-linux-gnueabi-gcc -D_OMAP5430 -D_SC_VER_1_16 -c -Wall -Wextra -Wno-missing-field-initializers -I -I. -Icommon -Ipmic -Iaudioic -Ilinux -Ii2c-tools -Iarch/arm/mach-omap/common -Iarch/arm/mach-omap/common/prcm -Iarch/arm/mach-omap/common/statcoll -Iarch/arm/mach-omap/omap4 -Iarch/arm/mach-omap/omap4/prcm -Iarch/arm/mach-omap/omap4/dpll -Iarch/arm/mach-omap/omap4/pmi -Iarch/arm/mach-omap/omap5 -Iarch/arm/mach-omap/omap5/prcm -Iarch/arm/mach-omap/omap5/dpll -Iarch/arm/mach-omap/omap5/ctrlmod -Iarch/arm/mach-omap/dra7 -Iarch/arm/mach-omap/dra7/ctrlmod -Iarch/arm/mach-omap/dra7/prcm -Iarch/arm/mach-omap/dra7/dpll -Iarch/arm/mach-omap/dra7/statcoll -Iarch/arm/mach-omap/am335x -Iarch/arm/mach-omap/am335x/prcm -Iarch/arm/mach-omap/am335x/dpll -static omapconf.c -o omapconf.o
make: arm-none-linux-gnueabi-gcc: Command not found
make: *** [omapconf.o] Error 127
Have I gone wrong somewhere or is there an alternate way for installing omapconf.
Thanks,
Rebel