Hello,
We are working on dra7xx-evm(OMAP5777) board. Here we are using these things:
1. linux-3.12 kernel
2. Toolchain- gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.
3. Filesystem- arago-glsdk-multimedia-image-dra7xx-evm.
4. glsdk_6.10.00.02
5. qt 5.1
6. kms display system for qt 5.1
We have successfully built qt 5.1 with opengl support for dra7xx-EVM. We have also tested opengl sample application (hellowindow ) using following command :
./hellowindow -qws -platform kms
Now we are trying to build and run another sample application hellogl_es2 (using QGLWidget), but it is giving error like :
load glyph failed err=24 face=0xf47a8
QOpenGLContext::makeCurrent() called with non-opengl surface 0xff840
QOpenGLContext::swapBuffers() called with non-opengl surface
Just for verification we did test application using QWidget (QLabel) to print "Welcome", and run it by following command:
./test -qws -platform kms
that result in following error:
load glyph failed err=24 face=0xf47a8
Note:- Same test application working with qt 4.8.4 without opengl support by following command :
./test -qws
Please help in this regard.
Regards,
Naveen