Hello,
We are working on dra7xx-evm(OMAP5777) board. Here we are using these things:
1. linux-3.12 kernel
2. Toolchain- gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.
3. glsdk_6.10.00.02
4. linuxutils_4_00_01_08
For the cmem support in linux3.12, we are trying to build linuxutils_4_00_01_08.
For building we have used the following setting in products.mak:
TOOLCHAIN_LONGNAME ?= arm-linux-gnueabihf
TOOLCHAIN_INSTALL_DIR ?= /home/mistral/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux
TOOLCHAIN_PREFIX ?= $(TOOLCHAIN_INSTALL_DIR)/bin/$(TOOLCHAIN_LONGNAME)-
KERNEL_INSTALL_DIR ?= /home/mistral/ti-glsdk_dra7xx-evm_6_10_00_02/board-support/linux
Then run the command to build the cmem library :
make -f lu.mak
make
For us cmem library built fine.
For building cmem module, we did the following:
cd linuxutils_4_00_01_08/src/cmem/module
make
But during building of cmem module we are getting the following error:
/home/mistral/ti-glsdk_dra7xx-evm_6_10_00_02/board-support/linux/arch//Makefile: No such file or directory
Complete error-log is in the below attached snapshot.
Please help in this regard.
Regards
Naveen